You probably do not come from: China. Click here for our other locations.

Gantry cranes less susceptible to defects

Monitoring and maintenance
Real-time maintenance Condition monitoring
Case Study

Increased system availability with condition monitoring solutions by ifm

Vibration data can be easily evaluated with sensors and software from ifm

Reliable monitoring of
critical STS crane areas

Maintenance service
via cloud solution possible

Results

  • Predictive maintenance for the port operators
  • High user-friendliness during integration and commissioning
  • Condition monitoring solution with the best price-performance ratio on the market
  • Cloud solution with ifm RTM software possible in the future

The challenge

Crane failures pose a major challenge for both port operators and crane manufacturers: When a crane fails, logistics comes to a standstill and high follow-up costs are engendered. Therefore, our customer aims to identify errors preferably at an early stage in order to prevent possible failu­res. In this context, various data are relevant and especially vibration data play an important role. In the past, they were faced with the problem that the vibration data could only be read out inefficiently.

Monitoring critical components in the STS crane’s machine room is essential for the early detection of problems. Unbalances may occur in drum bearings, gears and hoist motors. If the affected parts fail, the result is a plant standstill, which is often associated with high costs. By using sen­sor technology, however, these problems can be counteracted at an early stage.

Our customer

A manufacturer of gantry cranes that are used in the port industry with more than  800 employees is in use with its STS cranes in over 100 ports worldwide. Gantry cranes, aka ship-to-shore cranes as they are called in this industry, facilitate the port logistics and ensure the smooth handling of containers.

Our customer constantly strives to improve the productivity of their cranes in order to guarantee their customers an efficient and economic operation. In the daily routine of logistics remote access via the Cloud is gaining importance, for the port facilities are becoming increasingly complex which makes it hard to keep an overview of processes.

Our customer

A manufacturer of gantry cranes that are used in the port industry with more than  800 employees is in use with its STS cranes in over 100 ports worldwide. Gantry cranes, aka ship-to-shore cranes as they are called in this industry, facilitate the port logistics and ensure the smooth handling of containers.

Our customer constantly strives to improve the productivity of their cranes in order to guarantee their customers an efficient and economic operation. In the daily routine of logistics remote access via the Cloud is gaining importance, for the port facilities are becoming increasingly complex which makes it hard to keep an overview of processes.

The solution – why ifm?

Our customer‘s claim is to ensure crane opera­tion with as little downtime as possible for their customers. A condition monitoring solution to monitor critical components and thus prevent failures must be very easy to integrate into the existing systems and this is exactly what the sys­tems from ifm offer. VSA001 sensors and VSE100 evaluation units are used for this purpose, which allow a reliable analysis of critical machine areas. At the same time, the data is recorded over time.

The evaluation units monitor rolling bearings and gears for imbalances and thus enable a condi­tion-based maintenance in line with the compo­nent conditions. A total of four vibration sensors can be connected to one evaluation unit. This allows machine faults to be detected even before damage occurs. The system monitors certain fre­quencies making it possible to draw conclusions about the machine‘s condition. These frequen­cies are usually based on the speed of the shaft and the bearing types to be monitored.

Background vibrations that have no influence on the mode of operation are not taken into account. Alarm points can be set for each fre­quency. The measurement can refer to the speed, acceleration and distance, so that the monitoring data becomes even more meaningful. Our custo­mer can analyse the data remotely and provide a targeted maintenance service managed by gua­rantees and sales.

Case Study: Gantry cranes less susceptible to defects

The latest success stories

The inspiring application reports, case studies and video reports from all industries show how our customers successfully save costs with solutions from ifm. At the same time, the efficiency and functionality of machines can often be increased.