You probably do not come from: China. Click here for our other locations.

Aquafarming: Innovative solutions for efficient fish farms

Efficiency
Costs Material
Case Study

25 % faster project processing times with smart network technologies

36.000 €
Material cost savings

25 % Time savings
during commissioning

Additional measured values
in one device

Results

  • Material cost savings of more than € 36,000
  • 25 % time saved during commissioning
  • Increased safety through diagnostics at field device level
  • More accurate readings through digital communication

The challenge

Increasing environmental protection require­ments and acute international competition have created the need to constantly optimise fish farms. Technological innovations and a high­er degree of automation are required to save water and energy whilst increasing productivity. The growing number of sensors makes process control networking increasingly complex and time-consuming.

Aquafarms are very sensitive systems whose parameters must be continuously monitored. For example, to ensure healthy rearing of the fish, the water temperature and oxygen saturation must be at an appropriate level in all lines. One single wrong measurement can lead to the death of the entire fish population and cause signifi­cant financial loss. It is therefore of major impor­tance for aqua farm operators to install reliable sensors with long-term resistance to humid and salty air.

Our customer

A manufacturer of fish farming equipment

In addition to offshore farms in the sea, onshore farms are gaining in importance. Recirculating aquaculture systems (RAS) in particular offer the possibility of farming fish in an efficient resource-saving way. RAS technology meets strict environmen­tal regulations by treating polluted water so that it can be reused.

With fish farms for various species of freshwater and marine fish installed worldwide, our client is an expert in the sector of land-based fish farming..

Our customer

A manufacturer of fish farming equipment

In addition to offshore farms in the sea, onshore farms are gaining in importance. Recirculating aquaculture systems (RAS) in particular offer the possibility of farming fish in an efficient resource-saving way. RAS technology meets strict environmen­tal regulations by treating polluted water so that it can be reused.

With fish farms for various species of freshwater and marine fish installed worldwide, our client is an expert in the sector of land-based fish farming..

The solution – why ifm?

ifm offers fully digital network technology via IO-Link, with all sensors being connected (manu­facturer-independently) to the controller via field modules. Smart cabling with field modules in combination with M12 connectors reduces the installation time by 25 % and minimises the risk of errors. With the possibility of device diagnos­tics down to the field level, the customer not only achieves a higher safety standard, but the sensors can also report errors independently (e.g. wire break detection).

The extended functionality also means that addi­tional measured values are available from some sensors, e.g. the temperature for flow sensors, allowing the customer to save hundreds of tem­perature sensors initially included in the design.

The material cost savings achieved in this way add up to more than € 36,000 per plant. The ifm components’ high IP protection class and robust­ness provide the ideal basis for their long-lasting use in a harsh environment such as encountered in fish farming. The wide product range includ­ing sensors and network technology in combi­nation with their extensive consultation services and support make ifm a competent and reliable technology partner in the fish farming industry.

Case Study: Innovative solutions for efficient fish farms

The latest success stories

The inspiring application reports, case studies and video reports from all industries show how our customers successfully save costs with solutions from ifm. At the same time, the efficiency and functionality of machines can often be increased.